MfgTool Help

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MfgTool Help

1,949件の閲覧回数
nmmillward
Contributor I

Hi,

I'm trying to get the MfgTool (Version 1.6.2.048) to work with the i.MX28. I have followed the Manufacturing Tool Quick Start Guide document, supplied with the software, I only get so far.

After plugging the USB cable in, it auto installs as a HID-compliant device and a USB Input Device.

When I try to 'Scan devices' nothing happens, and when I try to open the USB configuration, by going to 'Options -> Configuration...' and then clicking the 'USB Ports' tab, the software crashes.

Any assistance or advice would be greatly appreciated.

ラベル(1)
0 件の賞賛
返信
1 返信

1,574件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nick

please check MFG Tool issues described on

p.20 MFG TOOL Customization Guide.pptx

Re: How to create your own Mfgtool firwmare

also there may be issues if computer has USB 3.0 controller,

it is recommended to disable it.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信