Message Queues

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Message Queues

3,484 次查看
jpe1313
Contributor II

I'm using the Yocto Freescale   core-image-base on the SABRE i.MX6 QUAD evaluation board.

I'd like to use message queues but they don't seem to be supported in this kernel?   Is that true or am I missing something?

THANKS IN ADVANCE

标签 (3)
3 回复数

3,089 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Janet Estabridis,

If you are referring to POSIX message queues these are not enabled by default, but you may use menuconfig to enable this function under General Setup > POSIX Message Queues.

There is more information on how to configure the kernel on the following document, which I'm sure will be very helpful.

https://community.nxp.com/docs/DOC-94196 

Regards,

0 项奖励
回复

3,089 次查看
jpe1313
Contributor II

When I click on the link it says

Unauthorized


Access to this place or content is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here.
CAN YOU HELP ME OUT?  I really want to enable the POSIX message queues and I've never recompiled a kernel for NXP.
Thanks
0 项奖励
回复

3,089 次查看
gusarambula
NXP TechSupport
NXP TechSupport

My apologies. Try this link instead:

https://community.nxp.com/docs/DOC-95045