May I use 4 data bit micro Card for i.mx6, SD card boot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

May I use 4 data bit micro Card for i.mx6, SD card boot?

Jump to solution
1,452 Views
MehmetAliIpin
Contributor V

Dear Sir/Madam,

Hello,

We are developing  an i.mx6 based system. We wish to boot from SD card. In the development kit, I see an 8 bit SD/MMC card connector is used and all 8 data bits are connected to it. But 8 bit SD/MMC card is not easy to find and may be expensive then 4 bit micro SD card connector. Therefore, if I use 4 bit micro SD card connector, shall I have U-boot/linux kernel problems to boot from 4 bit interface?

Best regards.

Mehmet Ali Ipin

Labels (1)
0 Kudos
Reply
1 Solution
1,112 Views
Yuri
NXP Employee
NXP Employee

  Please look at the following thread :

"I.mx6 board boot from micro-sd card( 8 data line or 4 data line) question?"

https://community.freescale.com/message/396151#396151

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,113 Views
Yuri
NXP Employee
NXP Employee

  Please look at the following thread :

"I.mx6 board boot from micro-sd card( 8 data line or 4 data line) question?"

https://community.freescale.com/message/396151#396151

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply