jitter specifications of CSI imput.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

jitter specifications of CSI imput.

858 Views
takashitakahash
Contributor III

Could you tell me jitter specification of BT.656 format in the video input to the CSI ?

IMX6DQAEC  of 4.11.10.3 Electrical Characteristics has been prescribed as 0.01 to 180 MHz pixel

clock input frequency range but not prescribed jitter specification .

<Phenomenon>

Display looks like normal, but a external video decoder isuees pixel clock varies as shown below .

It is a background that would you please make sure jitter can be allowed on the MX6D side.

Min.66.28-Typ.66.66MHz-Max.68.98MHz

Labels (2)
0 Kudos
Reply
1 Reply

794 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

jitter is not specified for CSI interface, that means

it is allowed, provided that signal complies with timing characteristics given in

Table 67. Sensor Interface Timing Characteristics IMX6DQCEC

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply