May I use 4 data bit micro Card for i.mx6, SD card boot?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

May I use 4 data bit micro Card for i.mx6, SD card boot?

ソリューションへジャンプ
1,394件の閲覧回数
MehmetAliIpin
Contributor V

Dear Sir/Madam,

Hello,

We are developing  an i.mx6 based system. We wish to boot from SD card. In the development kit, I see an 8 bit SD/MMC card connector is used and all 8 data bits are connected to it. But 8 bit SD/MMC card is not easy to find and may be expensive then 4 bit micro SD card connector. Therefore, if I use 4 bit micro SD card connector, shall I have U-boot/linux kernel problems to boot from 4 bit interface?

Best regards.

Mehmet Ali Ipin

ラベル(1)
0 件の賞賛
返信
1 解決策
1,054件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please look at the following thread :

"I.mx6 board boot from micro-sd card( 8 data line or 4 data line) question?"

https://community.freescale.com/message/396151#396151

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,055件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please look at the following thread :

"I.mx6 board boot from micro-sd card( 8 data line or 4 data line) question?"

https://community.freescale.com/message/396151#396151

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信