Maximum VPU power with minimal CPU and cost?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Maximum VPU power with minimal CPU and cost?

ソリューションへジャンプ
1,029件の閲覧回数
olegpereverzev
Contributor I

Hello, my application uses i.MX6Q as an CPU, but there is a need in live video transcoding. Using VPU of main unit is fine, but it allows only one thread, while we need three.

There is an obvious solution to use two more i.MX6S (as they are powerful  enough to transcode fullHD and cost less, than DSP), but is there even more cost-effective solution using VPU, like separate VPUs or low-power CPU with several VPUs?

ラベル(4)
タグ(3)
0 件の賞賛
返信
1 解決策
925件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Oleg

I am afraid there are no other special or non-standard solutions.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
926件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Oleg

I am afraid there are no other special or non-standard solutions.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
925件の閲覧回数
olegpereverzev
Contributor I

What a pity. Thanks though.

0 件の賞賛
返信