Maximum VPU power with minimal CPU and cost?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Maximum VPU power with minimal CPU and cost?

Jump to solution
1,028 Views
olegpereverzev
Contributor I

Hello, my application uses i.MX6Q as an CPU, but there is a need in live video transcoding. Using VPU of main unit is fine, but it allows only one thread, while we need three.

There is an obvious solution to use two more i.MX6S (as they are powerful  enough to transcode fullHD and cost less, than DSP), but is there even more cost-effective solution using VPU, like separate VPUs or low-power CPU with several VPUs?

Labels (4)
Tags (3)
0 Kudos
Reply
1 Solution
924 Views
igorpadykov
NXP Employee
NXP Employee

Hi Oleg

I am afraid there are no other special or non-standard solutions.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
925 Views
igorpadykov
NXP Employee
NXP Employee

Hi Oleg

I am afraid there are no other special or non-standard solutions.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
924 Views
olegpereverzev
Contributor I

What a pity. Thanks though.

0 Kudos
Reply