Maximum RAM size i.MX 8M can support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Maximum RAM size i.MX 8M can support

Jump to solution
4,096 Views
shuodo
Contributor II

Hi,

I would like to find out the maximum RAM size i.MX 8M can support.

I read the reference manual of IMX 8M. Section 2.1.2 A53 memory map, it says DDR memory size is 1 + 3 = 4GB:

A53-DDR-MEM.png

 

However, in section 9.1.1.1, DRAM interface summary says max up to 8GB of memory:

MAX-8GB.png

 

Which one is correct?

Or both are correct? They could be different things: one for DDR memory map size, the other one is for the max DDR size that DDR interface can support? If this is true, how could it handle map 8GB DDR into 4GB of memory space?

 

Best regards.

Tags (2)
0 Kudos
Reply
1 Solution
4,066 Views
joanxie
NXP TechSupport
NXP TechSupport

for imx8mq, the max density is 4G

View solution in original post

0 Kudos
Reply
3 Replies
4,080 Views
joanxie
NXP TechSupport
NXP TechSupport

do you mean imx8mm, imx8mn, imx8mq or imx8mp?

0 Kudos
Reply
4,078 Views
shuodo
Contributor II
0 Kudos
Reply
4,067 Views
joanxie
NXP TechSupport
NXP TechSupport

for imx8mq, the max density is 4G

0 Kudos
Reply