Max OSPI memory in iMx8 Quad Max

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Max OSPI memory in iMx8 Quad Max

Jump to solution
1,229 Views
ajmalmali
Contributor II

Hi

We are in the process of Processor analysis for a project. iMx8 Quad max is one of the major contenders. What is the max OSPI flash supported in iMx8QM. We see chips for up to 2Gb. Will this be supported in iMx8?

Regards

Tags (1)
0 Kudos
Reply
1 Solution
1,225 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ajmal

 

one can look at Table 5-19. FlexSPI Configuration block

sflashA1Size  4bytes   -..actual size, in terms of bytes  (the same is for i.MX8QM)

i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual

 

Best regards
igor

View solution in original post

0 Kudos
Reply
1 Reply
1,226 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ajmal

 

one can look at Table 5-19. FlexSPI Configuration block

sflashA1Size  4bytes   -..actual size, in terms of bytes  (the same is for i.MX8QM)

i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual

 

Best regards
igor

0 Kudos
Reply