Max OSPI memory in iMx8 Quad Max

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Max OSPI memory in iMx8 Quad Max

跳至解决方案
1,735 次查看
ajmalmali
Contributor II

Hi

We are in the process of Processor analysis for a project. iMx8 Quad max is one of the major contenders. What is the max OSPI flash supported in iMx8QM. We see chips for up to 2Gb. Will this be supported in iMx8?

Regards

标记 (1)
0 项奖励
回复
1 解答
1,731 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ajmal

 

one can look at Table 5-19. FlexSPI Configuration block

sflashA1Size  4bytes   -..actual size, in terms of bytes  (the same is for i.MX8QM)

i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,732 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ajmal

 

one can look at Table 5-19. FlexSPI Configuration block

sflashA1Size  4bytes   -..actual size, in terms of bytes  (the same is for i.MX8QM)

i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual

 

Best regards
igor

0 项奖励
回复