Mars Board booting from eMMC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Mars Board booting from eMMC

2,173 次查看
arunkumarjts
Contributor I

Hi all,
We are using the Mars board (i.MX6 Dual) for evaluation purpose using the android SDK.
We are able to flash the u-boot binary on SPI-NOR flash and Kernel and rootFS on eMMC partitions, using the MFG tool provided.
We are able to boot the Mars board using the above procedure.

However, we are trying to boot the u-boot binary from the eMMC (tried both on user partition and boot partition).
But the Mars board is not booted from the eMMC.

Note: We erased the u-boot binary present in the SPI-NOR flash.
Still, the board is not booted from the eMMC memory.

Reference:
User Manual : MarS Board User Manual_V1.1.pdf
MFG tool used : Mfgtools-Rel-12.04.01_ER_MX6Q_UPDATER

Please inform the procedure to boot the Mars board from the eMMC.

Thanks,
Arunkumar

标记 (2)
0 项奖励
回复
1 回复

2,027 次查看
winy2014
Contributor II

Forlinx also has i.MX6Q/DL and i.MX6UL which are all available for booting from eMMC or SD card.