Mars Board booting from eMMC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mars Board booting from eMMC

2,184件の閲覧回数
arunkumarjts
Contributor I

Hi all,
We are using the Mars board (i.MX6 Dual) for evaluation purpose using the android SDK.
We are able to flash the u-boot binary on SPI-NOR flash and Kernel and rootFS on eMMC partitions, using the MFG tool provided.
We are able to boot the Mars board using the above procedure.

However, we are trying to boot the u-boot binary from the eMMC (tried both on user partition and boot partition).
But the Mars board is not booted from the eMMC.

Note: We erased the u-boot binary present in the SPI-NOR flash.
Still, the board is not booted from the eMMC memory.

Reference:
User Manual : MarS Board User Manual_V1.1.pdf
MFG tool used : Mfgtools-Rel-12.04.01_ER_MX6Q_UPDATER

Please inform the procedure to boot the Mars board from the eMMC.

Thanks,
Arunkumar

タグ(2)
0 件の賞賛
返信
1 返信

2,038件の閲覧回数
winy2014
Contributor II

Forlinx also has i.MX6Q/DL and i.MX6UL which are all available for booting from eMMC or SD card.