Mars Board booting from eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mars Board booting from eMMC

2,192 Views
arunkumarjts
Contributor I

Hi all,
We are using the Mars board (i.MX6 Dual) for evaluation purpose using the android SDK.
We are able to flash the u-boot binary on SPI-NOR flash and Kernel and rootFS on eMMC partitions, using the MFG tool provided.
We are able to boot the Mars board using the above procedure.

However, we are trying to boot the u-boot binary from the eMMC (tried both on user partition and boot partition).
But the Mars board is not booted from the eMMC.

Note: We erased the u-boot binary present in the SPI-NOR flash.
Still, the board is not booted from the eMMC memory.

Reference:
User Manual : MarS Board User Manual_V1.1.pdf
MFG tool used : Mfgtools-Rel-12.04.01_ER_MX6Q_UPDATER

Please inform the procedure to boot the Mars board from the eMMC.

Thanks,
Arunkumar

Tags (2)
0 Kudos
Reply
1 Reply

2,046 Views
winy2014
Contributor II

Forlinx also has i.MX6Q/DL and i.MX6UL which are all available for booting from eMMC or SD card.