Making toaster working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Making toaster working

3,634 Views
Selea
Senior Contributor I
0 Kudos
Reply
3 Replies

2,625 Views
andreyreyes
Contributor II

Has anyone made any progress on this?

0 Kudos
Reply

2,625 Views
Selea
Senior Contributor I

First Problem:

to use toaster it says that it need django 1.5, but in the opensuse 12.3 (the one suggested) the last version is 1.4.8.... then it doesn't run the start script.

0 Kudos
Reply

2,625 Views
Selea
Senior Contributor I

This thread

is intented to start to working with toaster in yocto, Toaster is a webinterface to bitbake, to create, control and modify images (distributions) on imx6 (for me ).

I will start to post my progess in make the gui working, up to have a working tool to use bitbake in gui enviroment.

Well: at this time Toaster is just a GUi to see what bitbake isactually doing, but in the next release (1.7 probably), it will be possible also to create and configure images (as Hob does).

Omar

0 Kudos
Reply