CTS test vulnerable to BUG-21443020-WEBM crash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CTS test vulnerable to BUG-21443020-WEBM crash

Jump to solution
1,771 Views
björnqvarnström
Contributor II

When running CTS test android.security.cts.StagefrightTest we are getting an "Fatal signal 11 (SIGSEGV), code 1" error. We are running android 5.1.1 with the patches for BUG-21443020 added. The problem seams to occur when VPU frame memory is being freed. See attached Log. What could be the problem?

Original Attachment has been moved to: Log.txt.zip

Labels (2)
Tags (1)
0 Kudos
1 Solution
954 Views
björnqvarnström
Contributor II

Hi

You can find the patch attached to this mail.

/Björn

View solution in original post

4 Replies
954 Views
diegoadrian
NXP Employee
NXP Employee

Hello

I apologize for the late answer. I do not know if you still have a problem.

Unfortunately, there are reports that CTS test android.security.cts.StagefrightTest failed. There is a  "Fatal signal 11 (SIGSEGV), code 1" error:

"09-26 11:54:54.089 169 169 I DEBUG : signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr 0xb5000000:"[i.MX6Q][Android L5.1.1]CTS test failed: android.security.cts.StagefrightTest

As soon as the I can find a solution, I will let you know.

Best Regards,

Diego.

0 Kudos
954 Views
björnqvarnström
Contributor II

Hi

The problem was solved with the patch from Ankit Patel at NXP. So there is no longer an issue.

Regards

/Björn Qvarnström

0 Kudos
954 Views
diegoadrian
NXP Employee
NXP Employee

I am glad that the problem was solved.

However, is there a possibility, that you can share to us the patch?

This is because, if there are further problems of this issue. The patch could be a solution.

Best regards,

Diego.

0 Kudos
955 Views
björnqvarnström
Contributor II

Hi

You can find the patch attached to this mail.

/Björn