Making Initial code base for IMX7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Making Initial code base for IMX7

跳至解决方案
2,433 次查看
shashi_ray
Contributor II

Hi,

I am working on iMX7 dual processor with Yocto linux. To prepare the initial code base, there could be two options.

Option 1
Get the initial Yocto source code from yoctoproject git://git.yoctoproject.org/poky, checkout to any branch (preferably Sumo branch), add meta-freescale layer and do the yocto build and start working.
With this approach, kernel code is coming from git://github.com/Freescale/linux-fslc.git at  4.9-1.0.x-imx branch. 
 
 
Option 2 (as per Freescale_Yocto_Project_User's_Guide.pdf)
Get the initial Yocto code with repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1.15-1.0.0_ga and set up the project. 
With this approach, kernel code is coming from git://git.freescale.com/imx/linux-2.6-imx.git at branch imx_4.1.15_1.0.0_ga. But, the branch imx-4.1.15-1.0.0_ga seems very old.
Can someone please recommend me which option shall I choose to setup the code base and work further so that I should get all the latest  changes from NXP (Kernel change) as well as from Yocto project.
Thanks,
Shashi 
标签 (2)
0 项奖励
回复
1 解答
2,276 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Shashi

one can use both options, as for nxp releases one can look at latest L4.9.88 nxp bsp

linux-imx - i.MX Linux kernel 

Documentation

https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_LINUX_DOCS&Parent_nodeId=13376994810717061... 

i.MX Software|NXP 

https://community.nxp.com/message/402940#402940 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,276 次查看
shashi_ray
Contributor II

Thanks Igor

0 项奖励
回复
2,277 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Shashi

one can use both options, as for nxp releases one can look at latest L4.9.88 nxp bsp

linux-imx - i.MX Linux kernel 

Documentation

https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_LINUX_DOCS&Parent_nodeId=13376994810717061... 

i.MX Software|NXP 

https://community.nxp.com/message/402940#402940 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复