[MX8QM] HDMI Rx max resolution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[MX8QM] HDMI Rx max resolution

ソリューションへジャンプ
2,484件の閲覧回数
khang_letruong
Senior Contributor III

Hi NXP Teams,

I saw following sharing about enabling HDMI Rx in iMX8QM platform :

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-mx8qm-HDMI-RX/ta-p/1111058

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX8QM-How-to-enable-the-HDMI-RX-on-L5-1...

I have a use-case to read 4K HDMI camera input and I would like to know if this could be supported by the aforementioned platform, please ?

Thanks in advance and best regards,

Khang

 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,469件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

current bsp can support 4k@30

 

元の投稿で解決策を見る

3 返答(返信)
2,474件の閲覧回数
khang_letruong
Senior Contributor III

Hi again,

I read from the RM of iMX8QM that HDMI Rx can support 4K2K 60Hz :

MX8QM_HDMI_Rx.png

But I am not sure what is the current status of BSP.

Dear @joanxie ,

As author of one of previous sharing about the subject, would you have any additional information to provide, please ?

Thanks in advance and best regards,

Khang.

0 件の賞賛
返信
2,470件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

current bsp can support 4k@30

 

2,462件の閲覧回数
khang_letruong
Senior Contributor III

Thanks @joanxie for the confirmation!

K.

0 件の賞賛
返信