MX7 boundary scan requirements

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MX7 boundary scan requirements

跳至解决方案
1,352 次查看
demoniacmilk
Contributor IV

Hello!

If I want to use boundary scan on custom hardware, the following is necessary:

  1. PCIe domains must be powered (VP, VPH, VPTX)
  2. JTAG needs to be accessible
  3. JTAG_MOD is usually pulled down. This pulldown resistor needs to be removed for boundary scan functionality.

Are these the only requirements or is anything missing?

Thank you,

regards,
Lars

标签 (2)
0 项奖励
回复
1 解答
1,213 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Lars

yes these are only requirements, JTAG_MOD pull high and use

proper JTAG tools for boundary scan.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,214 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Lars

yes these are only requirements, JTAG_MOD pull high and use

proper JTAG tools for boundary scan.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复