MX7 boundary scan requirements

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX7 boundary scan requirements

Jump to solution
1,363 Views
demoniacmilk
Contributor IV

Hello!

If I want to use boundary scan on custom hardware, the following is necessary:

  1. PCIe domains must be powered (VP, VPH, VPTX)
  2. JTAG needs to be accessible
  3. JTAG_MOD is usually pulled down. This pulldown resistor needs to be removed for boundary scan functionality.

Are these the only requirements or is anything missing?

Thank you,

regards,
Lars

Labels (2)
0 Kudos
Reply
1 Solution
1,224 Views
igorpadykov
NXP Employee
NXP Employee

Hi Lars

yes these are only requirements, JTAG_MOD pull high and use

proper JTAG tools for boundary scan.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,225 Views
igorpadykov
NXP Employee
NXP Employee

Hi Lars

yes these are only requirements, JTAG_MOD pull high and use

proper JTAG tools for boundary scan.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply