MX6D hangs randomly on back-to-back reboot test with Android JB4.3_1.1.0 BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX6D hangs randomly on back-to-back reboot test with Android JB4.3_1.1.0 BSP

1,683 Views
YongJunChang
Contributor II

Hi all,

We are developing a system using MX6D (silicon rev 1.2) with Android JB4.3_1.1.0 BSP.

The system uses an 8bit eMMC as a boot source.

It has been looked working fine so far. But when we do a back-to-back reboot testing ( around 1sec term ), it hangs with the following message.

===============================================================================================================

CPU: Freescale i.MX6 family TO1.2 at 792 MHz
Thermal sensor with ratio = 179
Temperature:   36 C, calibration data 0x56d4c67d
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock     : 66000000Hz
ipg per clock : 66000000Hz
uart clock    : 80000000Hz
cspi clock    : 60000000Hz
ahb clock     : 132000000Hz
axi clock   : 264000000Hz
emi_slow clock: 132000000Hz
ddr clock     : 528000000Hz
usdhc1 clock  : 198000000Hz
usdhc2 clock  : 198000000Hz
usdhc3 clock  : 198000000Hz
usdhc4 clock  : 198000000Hz
nfc clock     : 24000000Hz
DRAM:   1 GB
MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3
csd is 0xd04f0132, 0xf5913ff, 0xffffffe7, 0x8a400000
*** Warning - bad CRC or MMC, using default environment

In:    serial
Out:   serial
Err:   serial
board_late_init : MMC_BOOT

kernel   @ 10808000 (3386112)
ramdisk  @ 11800000 (238506)
kernel cmdline:
        use uboot command line:
        arm_freq=800 console=ttymxc0,115200n8 init=/init video=mxcfb0:dev=ldb,SVGA,if=RGB24,ldb=sin0,fbpix=RGB32,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale ldo_active=on

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
[    0.000000] Initializing cgroup subsys cpu
[    0.000000] Linux version 3.0.35 (ychang@ubuntu) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #111 SMP Sun Jun 1 14:52:08 KST 2014
[    0.000000] Ignoring unrecognised tag 0x54410008
[    0.000000] Kernel command line: arm_freq=800 console=ttymxc0,115200n8 init=/init video=mxcfb0:dev=ldb,SVGA,if=RGB24,ldb=sin0,fbpix=RGB32,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale ldo_active=on
[    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Memory: 379MB 427MB = 806MB total
[    0.000000] Memory: 808552k/808552k available, 240024k reserved, 0K highmem
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     DMA     : 0xfbe00000 - 0xffe00000   (  64 MB)
[    0.000000]     vmalloc : 0xc0800000 - 0xf2000000   ( 792 MB)
[    0.000000]     lowmem  : 0x80000000 - 0xc0000000   (1024 MB)
[    0.000000]     pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)
[    0.000000]     modules : 0x7f000000 - 0x7fe00000   (  14 MB)
[    0.000000]       .init : 0x80008000 - 0x80039000   ( 196 kB)
[    0.000000]       .text : 0x80039000 - 0x805adf20   (5588 kB)
[    0.000000]       .data : 0x805ae000 - 0x805fd240   ( 317 kB)
[    0.000000]        .bss : 0x805fd264 - 0x8074f20c   (1352 kB)
[    0.000000] Hierarchical RCU implementation.
[    0.000000] NR_IRQS:624
[    0.000000] MXC GPIO hardware
[    0.000000] arm_max_freq=800MHz
[    0.000000] MXC_Early serial console at MMIO 0x2020000 (options '115200n8')
[    0.000000] bootconsole [ttymxc0] enabled
[    0.260351] Mount-cache hash table entries: 512
[    0.265685] Initializing cgroup subsys debug
[    0.269977] Initializing cgroup subsys cpuacct
[    0.274531] Initializing cgroup subsys freezer
[    0.279023] CPU: Testing write buffer coherency: ok
[    0.285057] Internal error: Oops - undefined instruction: 0 [#1] SMP
[    0.291435] Modules linked in:
[    0.294516] CPU: 0    Not tainted  (3.0.35 #111)
[    0.299156] PC is at search_extable+0x0/0x3c
[    0.303453] LR is at search_exception_tables+0x18/0x34
[    0.308611] pc : [<801c2b88>]    lr : [<80084a00>]    psr: 20000113
[    0.308617] sp : b0031d40  ip : b0031e68  fp : 00000009
[    0.320135] r10: 00000805  r9 : 20000113  r8 : 00000000
[    0.325377] r7 : b0024780  r6 : 00000000  r5 : b0031e68  r4 : 801c2534
[    0.331924] r3 : 00000001  r2 : 801c2534  r1 : 805ca870  r0 : 805c9ae0
[    0.338473] Flags: nzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment kernel
[    0.345804] Control: 10c53c7d  Table: 1000404a  DAC: 00000015
[    0.351568]
[    0.351570] PC: 0x801c2b08:
[    0.355860] 2b08  e92d4010 e59030b4 e3530000 0a00000c e59020b8 e590c0c0 e5921000 e15c0001
[    0.364176] 2b28  8a000007 e59040c8 e08cc004 e151000c 32822008 32433001 358020b8 358030b4
[    0.372501] 2b48  3affffef e59030b4 e3530000 08bd8010 e59020b8 e2433001 e59010c0 e7922183
[    0.380815] 2b68  e1510002 88bd8010 e590c0c8 e081100c e1520001 28bd8010 ffff30b4 eafffff0
[    0.389128] 2b88  fdf73000 ea000008 7fb7c001 e1a0c24c ff7b018c e793c18c e15c0002 32803008
[    0.397444] 2ba8  3a000001 912fff1e e2401008 e1530001 9afffff4 e3a00000 e12fff1e e92d4010
[    0.405759] 2bc8  e3a02001 e5903000 e201401f ea000004 e5b03004 e3530000 08bd8010 e1a012c1
[    0.414075] 2be8  e201401f e593c000 e18cc412 e583c000 e5933000 e3730001 0afffff4 e8bd8010
[    0.422392]
[    0.422395] LR: 0x80084980:
[    0.426685] 4980  e5930140 eaffffda e1a0200d e3c23d7f e3c3303f e593300c e5933294 e5931010
[    0.435002] 49a0  eaffffd3 e92d4070 e1a04000 e1a05001 e1a00004 e1a01005 ebfffdd3 e2506000
[    0.443314] 49c0  1a000004 e1a01004 e1a00005 ebfffe4c e2504000 cafffff5 e1a00006 e8bd8070
[    0.451628] 49e0  e2800008 eaff72ee e92d4010 e1a04000 e59f101c e1a02004 e59f0018 eb04f861
[    0.459941] 4a00  e3500000 18bd8010 e1a00004 e8bd4010 ea0063ce 805ca870 805c9ae0 e59f3050
[    0.468254] 4a20  e1500003 3a000003 e59f3048 e1500003 93a00001 912fff1e e59f303c e5933000
[    0.476564] 4a40  e3530000 13a00000 112fff1e e59f202c e1500002 3a000004 e59f3024 e1530000
[    0.484874] 4a60  33a00000 23a00001 e12fff1e e1a00003 e12fff1e 80008000 805adf20 805c3a20
[    0.493190]
[    0.493193] SP: 0xb0031cc0:
[    0.497484] 1cc0  59ffbefd 9fec9fd7 dbabc4ff fffffffd fcdeaffe 7fdcfedd daafd6ff fff7bf7d
[    0.505800] 1ce0  0000ffdf ffffffff b0031d2c b0030050 00000001 8003e184 805c9ae0 805ca870
[    0.514116] 1d00  801c2534 00000001 801c2534 b0031e68 00000000 b0024780 00000000 20000113
[    0.522430] 1d20  00000805 00000009 b0031e68 b0031d40 80084a00 801c2b88 20000113 ffffffff
[    0.530742] 1d40  b0031e68 80047d6c 00000805 80048124 0000fd7e fe6efeff 0000f97c d26ceb2f
[    0.539055] 1d60  b7fdfbfd de7cfffa f9cbfddd 00008000 00000000 900bdcb0 00000041 0003148e
[    0.547367] 1d80  805fc520 805fc520 00000000 00000000 80d50b78 00000000 00000000 800bdcb0
[    0.555678] 1da0  00000041 0003151c 00000805 805cbde4 00000000 b0031e68 805d78d8 20000113
[    0.563990]
[    0.563992] IP: 0xb0031de8:
[    0.568283] 1de8  40000013 805fc540 00000001 80d50c00 805fc520 800bf3b8 00000041 805fcfa0
[    0.576601] 1e08  00000000 00000002 000200d0 800bfb08 805fcfa4 00000000 805fc520 00000000
[    0.584917] 1e28  00000000 00000001 80d508a0 fffffffe 00000001 805fc520 00000000 000000d0
[    0.593229] 1e48  00000001 00000000 00004780 ffffffff b0031e9c 805d78d8 00000000 8003e06c
[    0.601542] 1e68  00000009 b000f000 0000ffff 00000000 805d78dc 00000008 805d78d8 00000000
[    0.609854] 1e88  805d78d8 00000009 00000000 00000009 00000000 b0031eb0 800845ac 801c2534
[    0.618165] 1ea8  20000013 ffffffff b0060000 b0061fb0 b00282e0 b00282fc 00000001 00000000
[    0.626479] 1ec8  b0060000 b0045b60 00800711 00000000 00000000 00000000 00000000 b0030000
[    0.634793]
[    0.634795] R0: 0x805c9a60:
[    0.639086] 9a60  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[    0.647398] 9a80  000001b8 00000000 00000000 00000000 00000000 00000000 00000000 5f4e4143
[    0.655710] 9aa0  004d4342 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[    0.664021] 9ac0  00000000 8042da94 00000000 00000000 00000000 00000000 00000000 00000000
[    0.672332] 9ae0  8003e380 80442da0 8003e388 80442da0 8003e398 80442da0 80040aa4 80442da4
[    0.680642] 9b00  80040ac0 80442dac 80040b40 80442db4 80040b4c 80442dbc 80040b58 80442dc4
[    0.688958] 9b20  80040b64 80442dcc 80040b70 80442dd4 80040b7c 80442ddc 80040b88 80442de4
[    0.697274] 9b40  80040b94 80442dec 80040ba0 80442df4 80040bac 80442dfc 80040bb8 80442e04
[    0.705591]
[    0.705593] R1: 0x805ca7f0:
[    0.709883] a7f0  801c1fe8 801c1ff8 801c1fec 801c1ff8 801c2408 804435b0 801c2444 804435c0
[    0.718197] a810  801ccb70 804435c8 801cd214 804435d4 80213214 804435e0 80213224 804435e8
[    0.726521] a830  8031f884 804435f0 8031f954 804435f8 8031fb58 80443600 8031fc80 80443608
[    0.734834] a850  8031fd50 80443610 8031ff78 80443618 803366cc 80443620 8033681c 80443628
[    0.743147] a870  8033683c 80443630 00000001 00000000 00000000 805ae000 00000002 00200000
[    0.751460] a890  00000000 00000000 00000000 00000000 00000078 00000078 00000078 00000000
[    0.759771] a8b0  80444338 00000000 00000400 00400000 00000000 00000000 00000000 805ca8cc
[    0.768082] a8d0  805ca8cc 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[    0.776395]
[    0.776398] R2: 0x801c24b4:
[    0.780689] 24b4  e0811100 e1a03312 f57ff05f e1912f9f e0120003 e0222003 e181cf92 e35c0000
[    0.789001] 24d4  1afffff9 f57ff05f e3500000 13a00001 e12fff1e e211c003 15cc1000 e3a02001
[    0.797315] 24f4  e200301f e1a002a0 e0811100 e1a03312 f57ff05f e1912f9f e0120003 11c22003
[    0.805627] 2514  e181cf92 e35c0000 1afffff9 f57ff05f e3500000 13a00001 e12fff1e e211c003
[    0.813939] 2534  15cc1000 e3a02001 e200301f e1a002a0 e0811100 e1a03312 f57ff05f e1912f9f
[    0.822251] 2554  e0120003 01822003 e181cf92 e35c0000 1afffff9 f57ff05f e3500000 13a00001
[    0.830564] 2574  e12fff1e e1510003 01500002 33a00000 03a00001 83a00002 e1a0f00e e1510003
[    0.838877] 2594  01500002 33e00000 03a00000 83a00001 e1a0f00e e92d4038 e1a04000 e1a05000
[    0.847189]
[    0.847192] R4: 0x801c24b4:
[    0.851482] 24b4  e0811100 e1a03312 f57ff05f e1912f9f e0120003 e0222003 e181cf92 e35c0000
[    0.859796] 24d4  1afffff9 f57ff05f e3500000 13a00001 e12fff1e e211c003 15cc1000 e3a02001
[    0.868109] 24f4  e200301f e1a002a0 e0811100 e1a03312 f57ff05f e1912f9f e0120003 11c22003
[    0.876421] 2514  e181cf92 e35c0000 1afffff9 f57ff05f e3500000 13a00001 e12fff1e e211c003
[    0.884731] 2534  15cc1000 e3a02001 e200301f e1a002a0 e0811100 e1a03312 f57ff05f e1912f9f
[    0.893044] 2554  e0120003 01822003 e181cf92 e35c0000 1afffff9 f57ff05f e3500000 13a00001
[    0.901358] 2574  e12fff1e e1510003 01500002 33a00000 03a00001 83a00002 e1a0f00e e1510003
[    0.909670] 2594  01500002 33e00000 03a00000 83a00001 e1a0f00e e92d4038 e1a04000 e1a05000
[    0.917983]
[    0.917986] R5: 0xb0031de8:
[    0.922276] 1de8  40000013 805fc540 00000001 80d50c00 805fc520 800bf3b8 00000041 805fcfa0
[    0.930589] 1e08  00000000 00000002 000200d0 800bfb08 805fcfa4 00000000 805fc520 00000000
[    0.938901] 1e28  00000000 00000001 80d508a0 fffffffe 00000001 805fc520 00000000 000000d0
[    0.947212] 1e48  00000001 00000000 00004780 ffffffff b0031e9c 805d78d8 00000000 8003e06c
[    0.955524] 1e68  00000009 b000f000 0000ffff 00000000 805d78dc 00000008 805d78d8 00000000
[    0.963836] 1e88  805d78d8 00000009 00000000 00000009 00000000 b0031eb0 800845ac 801c2534
[    0.972149] 1ea8  20000013 ffffffff b0060000 b0061fb0 b00282e0 b00282fc 00000001 00000000
[    0.980459] 1ec8  b0060000 b0045b60 00800711 00000000 00000000 00000000 00000000 b0030000
[    0.988770]
[    0.988773] R7: 0xb0024700:
[    0.993064] 4700  8060233c b0024704 b0024704 00000000 b0024710 b0024710 00000000 00000000
[    1.001376] 4720  00000000 00000001 00000000 b002472c b002472c 00000000 b0024738 b0024738
[    1.009688] 4740  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[    1.017998] 4760  0000c350 0000c350 00000000 00000001 ffffff7e efffffdf ffbddffe fb7f9ffe
[    1.026311] 4780  00000000 b0030000 00000002 80208040 00000000 00000000 00000001 00000001
[    1.034621] 47a0  00000078 00000078 00000078 00000000 80444278 00000000 00000400 00400000
[    1.042932] 47c0  00000001 00000000 00000000 80f570b8 80f570b8 00000001 10fd3288 00000000
[    1.051244] 47e0  0004f1a1 00000000 00ef3e6f 00000000 0004967b 00000000 00000000 00000000
[    1.059560] Process kthreadd (pid: 2, stack limit = 0xb00302f0)
[    1.065498] Stack: (0xb0031d40 to 0xb0032000)
[    1.069875] 1d40: b0031e68 80047d6c 00000805 80048124 0000fd7e fe6efeff 0000f97c d26ceb2f
[    1.078093] 1d60: b7fdfbfd de7cfffa f9cbfddd 00008000 00000000 900bdcb0 00000041 0003148e
[    1.086299] 1d80: 805fc520 805fc520 00000000 00000000 80d50b78 00000000 00000000 800bdcb0
[    1.094506] 1da0: 00000041 0003151c 00000805 805cbde4 00000000 b0031e68 805d78d8 20000113
[    1.102711] 1dc0: 00000000 800393d8 0000cfa4 00000000 0000c520 805fc520 00000000 00000001
[    1.110918] 1de0: 00000001 805fc520 40000013 805fc540 00000001 80d50c00 805fc520 800bf3b8
[    1.119123] 1e00: 00000041 805fcfa0 00000000 00000002 000200d0 800bfb08 805fcfa4 00000000
[    1.127329] 1e20: 805fc520 00000000 00000000 00000001 80d508a0 fffffffe 00000001 805fc520
[    1.135535] 1e40: 00000000 000000d0 00000001 00000000 00004780 ffffffff b0031e9c 805d78d8
[    1.143741] 1e60: 00000000 8003e06c 00000009 b000f000 0000ffff 00000000 805d78dc 00000008
[    1.151946] 1e80: 805d78d8 00000000 805d78d8 00000009 00000000 00000009 00000000 b0031eb0
[    1.160153] 1ea0: 800845ac 801c2534 20000013 ffffffff b0060000 b0061fb0 b00282e0 b00282fc
[    1.168358] 1ec0: 00000001 00000000 b0060000 b0045b60 00800711 00000000 00000000 00000000
[    1.176564] 1ee0: 00000000 b0030000 b0045c7c 8006d2b4 b0031f80 b002b068 80f57088 00000000
[    1.184769] 1f00: b0031f80 00000000 80f57040 00000000 b002b060 00000000 00800711 b0031f80
[    1.192974] 1f20: 00000000 00000000 00000000 00000000 00000000 8006d9f0 00000000 00000000
[    1.201180] 1f40: 00000000 bff7ffbf fbf7dfad dbebfffa 800871bc 800371b4 80038040 80086ef8
[    1.209386] 1f60: b002ff30 00000611 b002ff30 00000000 8060114c 8003f100 00000000 00000000
[    1.217591] 1f80: 00000000 00000000 00000000 00000000 b002ff30 80086ef8 8003f034 00000013
[    1.225796] 1fa0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 8003f024
[    1.234002] 1fc0: 00000093 00000000 b002ff50 805d79fc b0030000 80087210 00000000 00000000
[    1.242208] 1fe0: 80087150 8003f034 00000013 00000000 00000000 8003f034 febfff7c fff9fbb7
[    1.250430] [<801c2b88>] (search_extable+0x0/0x3c) from [<80084a00>] (search_exception_tables+0x18/0x34)
[    1.259962] [<80084a00>] (search_exception_tables+0x18/0x34) from [<80047d6c>] (fixup_exception+0x10/0x28)
[    1.269657] [<80047d6c>] (fixup_exception+0x10/0x28) from [<80048124>] (do_page_fault+0x254/0x28c)
[    1.278655] [<80048124>] (do_page_fault+0x254/0x28c) from [<800393d8>] (do_DataAbort+0x34/0x98)
[    1.287394] [<800393d8>] (do_DataAbort+0x34/0x98) from [<8003e06c>] (__dabt_svc+0x4c/0x60)
[    1.295683] Exception stack(0xb0031e68 to 0xb0031eb0)
[    1.300754] 1e60:                   00000009 b000f000 0000ffff 00000000 805d78dc 00000008
[    1.308960] 1e80: 805d78d8 00000000 805d78d8 00000009 00000000 00000009 00000000 b0031eb0
[    1.317163] 1ea0: 800845ac 801c2534 20000013 ffffffff
[    1.322253] [<8003e06c>] (__dabt_svc+0x4c/0x60) from [<801c2534>] (_test_and_set_bit+0x4/0x48)
[    1.330896] Code: e1520001 28bd8010 e58030b4 eafffff0 (e1a03000)
[    1.337054] ---[ end trace 1b75b31a2719ed1c ]---

===============================================================================================================

It happens at very different locations and with different oops messages whenever the system hangs.

Do you guys have any suspicicous things on it?

Thanks in advance so much!

Labels (2)
Tags (3)
0 Kudos
Reply
1 Reply

1,152 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yong

errors at different locations may mean

DDR errors, may be useful to update calibration coefficients

with links below

https://community.freescale.com/message/331721#331721

https://community.freescale.com/docs/DOC-96412

Just for test one can try to boot with lower frequency using fuse

BT_FREQ (BOOT_CFG3[2]) and increase pause between boots.

This may check if problem is related to power supplies (poor filtering, noise)

problems.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply