MX50: Precaution when using SPI in slave mode -blog archive

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MX50: Precaution when using SPI in slave mode -blog archive

902件の閲覧回数
PeterChan
NXP Employee
NXP Employee

If you have read the IMX50 chip errata, you may note that there are several issues related to the eCSPI and CSPI in slave mode. Do not attempt to transmit data more than the BURST_LENGTH. The SPI will continue to consume your TX data buffer after BURST_LENGTH is reached it will transmit corrupted data when BURST_LENGTH is crossed.

 

 

タグ(1)
0 件の賞賛
返信
0 返答(返信)