MX28: Using Mfgtool with Mainline kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MX28: Using Mfgtool with Mainline kernel

跳至解决方案
5,164 次查看
lategoodbye
Senior Contributor I

Hi,

i want to use a recent Linux kernel as an updater linux for Mfgtool on custom MX28 board. I succeeded to port the FSL_UTP_UPDATER into Kernel 4.2.5, but the performance is bad (FSL 2.6.35 takes 4 minutes and Kernel 4.2.5 takes 11 minutes).

Any ideas what could be the reason for this?

标签 (2)
标记 (2)
0 项奖励
回复
1 解答
4,977 次查看
lategoodbye
Senior Contributor I

I solved it. It was a combination of multiple issues:

  • suboptimal Kernel config
  • wrong version of FSL updater
  • missing DDR support in MMC driver
  • disabled streaming in Chipidea UDC driver

在原帖中查看解决方案

0 项奖励
回复
2 回复数
4,975 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Stefan

FSL 2.6.35 and 3.0.35 (please check attached Linux Manuals USB Chapters)

use ARC USB Driver, while 4.1.15  - CHIPIDEA USB Driver, so probably

this may be a reason.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
4,978 次查看
lategoodbye
Senior Contributor I

I solved it. It was a combination of multiple issues:

  • suboptimal Kernel config
  • wrong version of FSL updater
  • missing DDR support in MMC driver
  • disabled streaming in Chipidea UDC driver
0 项奖励
回复