MX1 bare-metal example code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MX1 bare-metal example code

ソリューションへジャンプ
2,823件の閲覧回数
samcheck
NXP Employee
NXP Employee

I need to resurrect UART 2 on the MC9328MX1

All the code supporting that UART was removed and a couple years later all the code was migrated from one version control system to another. 

I know the odds are pretty long for efficiently bringing up a peripheral with only the manual for help.  Do you know of a bare-metal example that uses UART 2 without just using an OS’s drivers that I don’t have?

0 件の賞賛
返信
1 解決策
2,730件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Samuel

please look at attached file.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,731件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Samuel

please look at attached file.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,730件の閲覧回数
samcheck
NXP Employee
NXP Employee

Thank you!

0 件の賞賛
返信