Hi,
I am using a iMX8QxP MEK evaluation board and I would like to use NXP i.MX/Mscale DDR Tool V3.20.
- The MEK eval board is in Serial mode (switches: 0001)
- I open Mscale as administrator on a Windows PC
- I plug USB-C from the MEK eval board to the Win PC: on the Device Manager window, I can see HID-compliant device + USB Input device displayed
- I plug the debug USB from the MEK eval board to the Win PC: now, when I click "Search" button of the Mscale window, I can see 4 COMs.
- In the Mscale window:
o I select one of the 4 COMs
o I click on "Connect" button
o I select a DDR script (for example,.../script/mx8m/mx8m_micron_lpddr4_3gb_2d_1600m_200m_50m_32bit_RPAv25.ds)
o Target =MX8M, Clock=Default, DDR=LPDDR4, Density=Default (values by default but are they correct?)
o I click on "Download" button
I have this message:
ERROR: Can't open USB device!!!
Please check if the correct target is selected and set to the serial download mode.
I tried with the 4 COMs, same result.
I tried with another PC, same result.
I am sure the MEK board is in serial mode as I can use uuu to download a new program.
Is my Mscale version correct? (V3.20)
I run out of ideas... If you have any suggestions, please tell me.