MP3/AAC decoding problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MP3/AAC decoding problem

跳至解决方案
2,575 次查看
henri_bragge
Contributor II

When playing MP3/AAC/OGG audio files with gplay, audio keeps a crackling noise. This only happens on my custom image. FSL default image (X11 11.09.01 image) works OK. I have verified that gstreamer/alsa/gst-plugins and all other versions are identical in my image, but haven't found any meaningful difference. Just wondering if anyone else has had the same problem, and could provide some hints?


My HW is MX53 QSB, and kernel 2.35.3.

 

I attached gplay debug output with GST_DEBUG=2 (gplay-mp3.txt) and GST_DEBUG=3 (gplay-mp3-full.txt). Some warnings exist, but they also occur on FSL image that has no audible decoding problems.

Original Attachment has been moved to: gplay-mp3.txt.zip

Original Attachment has been moved to: gplay-mp3-full.txt.zip

标签 (3)
0 项奖励
回复
1 解答
2,135 次查看
adrian_alonso
NXP Employee
NXP Employee

Hi,

You could review how open source community is integrating and generating a custom BSP where that have support for

iMX53 QSB and you could take as reference to compare it with your integration process.

Freescale/fsl-community-bsp-platform · GitHub

From your log files seem that is a more likely a gstreamer related error, compare the build options used in Ltib base release, Yoctoproject and your custom BSP.

Regards

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,136 次查看
adrian_alonso
NXP Employee
NXP Employee

Hi,

You could review how open source community is integrating and generating a custom BSP where that have support for

iMX53 QSB and you could take as reference to compare it with your integration process.

Freescale/fsl-community-bsp-platform · GitHub

From your log files seem that is a more likely a gstreamer related error, compare the build options used in Ltib base release, Yoctoproject and your custom BSP.

Regards

0 项奖励
回复