MMPF0200 output capacitor values

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MMPF0200 output capacitor values

1,333 次查看
vadimaleynikov
Contributor III

Hello,

Is it correct/possible to decrease the SW1A/B and SW3A/B output capacitors to 2x22uF each when the maximum loads of these regulators are limited to 1A?

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

1,131 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vadim

I believe this is possible, in particular this option is mentioned in

MMPF0200 Table 70. SW3A/B External Component Requirements

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,131 次查看
vadimaleynikov
Contributor III

Hi Igor,

Thank you. Unfortunately your reference to Table 70 is applicable to SW3A/B only and I'm not sure if the SW1A/B feedback loop is stable with 2x22uF output capacitors.

Best regards,

Vadim

0 项奖励
回复