MMPF0200 output capacitor values

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMPF0200 output capacitor values

1,935 Views
vadimaleynikov
Contributor III

Hello,

Is it correct/possible to decrease the SW1A/B and SW3A/B output capacitors to 2x22uF each when the maximum loads of these regulators are limited to 1A?

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

1,733 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vadim

I believe this is possible, in particular this option is mentioned in

MMPF0200 Table 70. SW3A/B External Component Requirements

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,733 Views
vadimaleynikov
Contributor III

Hi Igor,

Thank you. Unfortunately your reference to Table 70 is applicable to SW3A/B only and I'm not sure if the SW1A/B feedback loop is stable with 2x22uF output capacitors.

Best regards,

Vadim

0 Kudos
Reply