MMPF0100NPZES Coin Mode Current Draw

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMPF0100NPZES Coin Mode Current Draw

1,754 Views
TerryMcHenry
Contributor II

When the system is in Coin Cell mode, with Vin = 0V, the current drawn by the LICELL pin (VSNVS_3V Domain) is around 75 uA, but after about two minutes this current increases to 180 uA and then slowly returns to 75 uA.

Is normal/acceptable?  What is happening?

Tags (2)
0 Kudos
Reply
2 Replies

1,580 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Terry McHenry,

What could be happening here is that additional current may be drawn in the coin cell mode when RESETBMCU is pulled up to VSNVS due an internal path from RESETBMCU to VIN and this could be seen as a normal known behavior.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,580 Views
CarlosCasillas
NXP Employee
NXP Employee

reyes, could you please check?

0 Kudos
Reply