MMPF0100NPZES Coin Mode Current Draw

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMPF0100NPZES Coin Mode Current Draw

1,775件の閲覧回数
TerryMcHenry
Contributor II

When the system is in Coin Cell mode, with Vin = 0V, the current drawn by the LICELL pin (VSNVS_3V Domain) is around 75 uA, but after about two minutes this current increases to 180 uA and then slowly returns to 75 uA.

Is normal/acceptable?  What is happening?

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,601件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Terry McHenry,

What could be happening here is that additional current may be drawn in the coin cell mode when RESETBMCU is pulled up to VSNVS due an internal path from RESETBMCU to VIN and this could be seen as a normal known behavior.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,601件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

reyes, could you please check?

0 件の賞賛
返信