MMPF0100F3AEP LiCell Pin Connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMPF0100F3AEP LiCell Pin Connection

1,471 Views
pankajrana
Contributor III

Hi,

In a design including i.Mx6 SoloLite Processor,with PMIC version "MMPF0100F3AEP" and without any Coin Cell, whether do we need to bypass with a 0.1uF to ground , or do we need to connect the pin to a valid voltage source ?

Regards,

Pankaj Rana

Labels (1)
0 Kudos
Reply
1 Reply

1,333 Views
art
NXP Employee
NXP Employee

You can just bypass the LICELL pin to ground through a 0.1uF capacitor and do nothing else.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply