MMPF0100F3AEP LiCell Pin Connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMPF0100F3AEP LiCell Pin Connection

1,443件の閲覧回数
pankajrana
Contributor III

Hi,

In a design including i.Mx6 SoloLite Processor,with PMIC version "MMPF0100F3AEP" and without any Coin Cell, whether do we need to bypass with a 0.1uF to ground , or do we need to connect the pin to a valid voltage source ?

Regards,

Pankaj Rana

ラベル(1)
0 件の賞賛
返信
1 返信

1,305件の閲覧回数
art
NXP Employee
NXP Employee

You can just bypass the LICELL pin to ground through a 0.1uF capacitor and do nothing else.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信