MMPF0100 pre-programmed OTP value is different with datasheet.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMPF0100 pre-programmed OTP value is different with datasheet.

1,956件の閲覧回数
seongkeunjin
Contributor II


Hi.

I'm using MMPF0100(F0 code) for i.MX6Q device. I have a question about pre-programmed OTP value.

I confirmed that VGEN4 VOUT is 1.8V at F0 code device. But I met 3.0V on VGEN4 VOUT on my board.

Others are OK. Only VGEN4 is wrong. Is it possible?

I attached OTP table below.

mmpf0100_otp_table.jpg

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,787件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  let me look at the schematic.

You may create request for it : How to submit a new question for NXP Support

Also, please check Your design regarding ER19 from the PMIC Errata.

"When VIN starts, it ramps up from between 100 mV and

400 mV, the regulators may not startup and/or the buck regulator

outputs can glitch high momentarily."

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,787件の閲覧回数
seongkeunjin
Contributor II

Here is my schematic. Please review it.

sch_mmpf.GIF

0 件の賞賛
返信