MMPF0100 pre-programmed OTP value is different with datasheet.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MMPF0100 pre-programmed OTP value is different with datasheet.

1,991 次查看
seongkeunjin
Contributor II


Hi.

I'm using MMPF0100(F0 code) for i.MX6Q device. I have a question about pre-programmed OTP value.

I confirmed that VGEN4 VOUT is 1.8V at F0 code device. But I met 3.0V on VGEN4 VOUT on my board.

Others are OK. Only VGEN4 is wrong. Is it possible?

I attached OTP table below.

mmpf0100_otp_table.jpg

标记 (1)
0 项奖励
回复
2 回复数

1,822 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  let me look at the schematic.

You may create request for it : How to submit a new question for NXP Support

Also, please check Your design regarding ER19 from the PMIC Errata.

"When VIN starts, it ramps up from between 100 mV and

400 mV, the regulators may not startup and/or the buck regulator

outputs can glitch high momentarily."

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,822 次查看
seongkeunjin
Contributor II

Here is my schematic. Please review it.

sch_mmpf.GIF

0 项奖励
回复