MIPI interface on iMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIPI interface on iMX6

1,766件の閲覧回数
gsr
Contributor I

Hi,

I am designing a  product with iMX6 solo and have a question about MIPI interface. Does anybody have any experience of the maximum length of FPC(flexi cable)of camera  that could work with MIPI interface on iMX6?

Our current form factor of the product requires FPC equivalent to 24cm.If my design   matches impedance of transmission lines well, would that work?

Any help would be highly appreciated.

Thanks,

GSR

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,604件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Gul

this may depend on data rate and strictly speaking, require simulations.

One can refer below for some estimations

http://www.emc.polito.it/SPI07/Presentations/May_tue_15/Session_8_PM/PresentationSPI.pdf

http://www.ti.com/lit/ml/snla187/snla187.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,604件の閲覧回数
gsr
Contributor I

HI igor,

Thanks for useful information. I will try to simulate and see how it goes?

Regards,

Gul

0 件の賞賛
返信