MIPI DSI max display resolution

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MIPI DSI max display resolution

跳至解决方案
4,469 次查看
jotes
Contributor IV

What is the maximum display resolution for MIPI DSI?

Is it 1280x720 (as it is mentioned in IMX6DQRM Rev. 3, 07/2015) or is it 1024x768 (IMX6QLXRM Rev L3.0.35_4.1.0, 09/2013)?

We would like to connect the 1280x720 Super AMOLED display to our IMX6Q board, and we wonder if it has any chance to work correctly?

0 项奖励
回复
1 解答
3,337 次查看
art
NXP Employee
NXP Employee

The maximum possible display resolution on the MIPI DSI interface of the i.MX6Dual/Quad processors is 1280x720 pixels, as specified in the Reference Manual document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
3,338 次查看
art
NXP Employee
NXP Employee

The maximum possible display resolution on the MIPI DSI interface of the i.MX6Dual/Quad processors is 1280x720 pixels, as specified in the Reference Manual document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复