MIPI Camera capture on ubuntu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI Camera capture on ubuntu

3,297 Views
ahmedtolba
Contributor I

Hi All,

I would like to ask if its possible to use/ capture the data from the mipi-csi2 port on ubuntu using your current driver and mx6?

I would like to just capture it  without v4l2, just want to capture pure packets then use SDL or any OpenGL to render the data

Labels (2)
0 Kudos
Reply
3 Replies

2,279 Views
daiane_angolini
NXP Employee
NXP Employee

I would start trying unit_test capture test.

Do you have the folder /unit_test?

find for some test with capture within the name.

Then you can try to capture something using your camera. What camera are you using?

0 Kudos
Reply

2,279 Views
ahmedtolba
Contributor I

I don't have a unit test.

I'm using  Samsung 5Mpixel K5ECG MIPI CSI sensor

0 Kudos
Reply

2,279 Views
daiane_angolini
NXP Employee
NXP Employee

So, find the unit_test and use ti.

I think you would need to install it. (sorry, I´m not used with Ubuntu rootfs)