MIPI CSI2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIPI CSI2

2,967件の閲覧回数
simon6
Contributor I

Hi,

Is there a guide similar to the AN5305 (which is for iMX6) for the iMX8MQ?

It would be greatly appreciated,

Thanks,

Simon P. Tsaoussis

ラベル(1)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,849件の閲覧回数
simon6
Contributor I

At the very least is there some information that can help me with the questions asked in: Camera porting guide for MIPI-CSI2 on i.MX8M?  about the clock rates?  Because I found this in the iMX8M docs: pastedImage_2.png

But this does not state anything about relationships or limits of the clocks to each other. How do I know my clock configuration is valid?

0 件の賞賛
返信

2,849件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

afaik most detailed info was provided by Tom Zheng on :

Fixing 'base address switching Change Err' which occurs randomly 

Best regards
igor

0 件の賞賛
返信

2,849件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Simon

unfortunately such documentation is not available, sorry.

May be useful to look at linux mipi csi drivers descriptions in

Linux 4.19.35_1.1.0 Documentation

[v9,2/2] phy: Add driver for mixel mipi dphy found on NXP's i.MX8 SoCs - Patchwork 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信