MIPI CSI2 without I2C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI CSI2 without I2C

2,219 Views
DYD
Contributor I

Hi all, 

For a project I am connecting a camera with a Google Coral board (imx8 running Mendel). However, the camera does not run the MIPI protocol but a parallel protocol. Hence, there is a bridge which converts to MIPI. But this means that there is no way of communicating with the camera with I2C. So we will have to write a custom driver for it without the I2C. We are already looking at the v4l2 to do this. 

Because we have zero experience doing this, we wonder if there are any examples which we can look into, and where they are. 

Thanks in advance!!

0 Kudos
Reply
1 Reply

2,192 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yannick

 

one can look at below thread with links to some examples

https://community.nxp.com/t5/i-MX-Processors/Parallel-video-on-IPU0-CSI-Input-without-I2C/td-p/12913...

 

Best regards
igor

Tags (1)
0 Kudos
Reply