MIPI CSI2 without I2C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MIPI CSI2 without I2C

2,028 次查看
DYD
Contributor I

Hi all, 

For a project I am connecting a camera with a Google Coral board (imx8 running Mendel). However, the camera does not run the MIPI protocol but a parallel protocol. Hence, there is a bridge which converts to MIPI. But this means that there is no way of communicating with the camera with I2C. So we will have to write a custom driver for it without the I2C. We are already looking at the v4l2 to do this. 

Because we have zero experience doing this, we wonder if there are any examples which we can look into, and where they are. 

Thanks in advance!!

0 项奖励
回复
1 回复

2,001 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yannick

 

one can look at below thread with links to some examples

https://community.nxp.com/t5/i-MX-Processors/Parallel-video-on-IPU0-CSI-Input-without-I2C/td-p/12913...

 

Best regards
igor

标记 (1)
0 项奖励
回复