MIPI -CSI2 Interface with i.MX8QM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIPI -CSI2 Interface with i.MX8QM

2,310件の閲覧回数
sameer_pitre
Contributor II

Hi,

I want to interface Sony LVDS camera to i.MX 8Q MAX processor. I want to use Lattice Crosslink ( D-PHY Revision 1.1 ) device as bridge for LVDS to MIPI-CSI2 conversion. The Crosslink D-PHY is 1.2V versus i.MX8M 1.0V.

My question is can I use the Crosslink device without any issue ?

BR,

Sameer

 

2 返答(返信)

2,150件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

it is likely to work, but would recommend asking Lattice to comment on the different operating voltage conditions to be sure.

2,150件の閲覧回数
sameer_pitre
Contributor II

Hi Joan,

Thanks. I had asked Lattice already. They think it should work. The VIH and VIL levels for the Crosslink device MIPI D-PHY are as follows, ( MIN, TYP, MAX)

pastedImage_1.png

BR,

Sameer

0 件の賞賛
返信