MIPI CSI Virtual Channel 3 support 3.10.17 Kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MIPI CSI Virtual Channel 3 support 3.10.17 Kernel

跳至解决方案
2,685 次查看
saurabh206
Senior Contributor III

Hi,

I am trying to enable MIPI CSI Virtual channel 3 support on 3.10.17 kernel.

I have followed the Sample code for iMX6 SabreSD to use MIPI CSI camera with virtual channel 3.

Still I am getting " mipi csi2 can not receive sensor clk1'

How to solve this issue?

Thanks

Saurabh

标签 (1)
1 解答
2,282 次查看
saurabh206
Senior Contributor III

I am able to fixed this issue.

It was hardware issue.

Following patch is the only modification required for Virtual channel 3.

Sample code for iMX6 SabreSD to use MIPI CSI camera with virtual channel 3.

Thanks

Saurabh

在原帖中查看解决方案

2 回复数
2,283 次查看
saurabh206
Senior Contributor III

I am able to fixed this issue.

It was hardware issue.

Following patch is the only modification required for Virtual channel 3.

Sample code for iMX6 SabreSD to use MIPI CSI camera with virtual channel 3.

Thanks

Saurabh

2,282 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Saurabh ,

   Good job !

Weidong

0 项奖励
回复