MIPI CSI Virtual Channel 3 support 3.10.17 Kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIPI CSI Virtual Channel 3 support 3.10.17 Kernel

ソリューションへジャンプ
1,216件の閲覧回数
saurabh206
Senior Contributor III

Hi,

I am trying to enable MIPI CSI Virtual channel 3 support on 3.10.17 kernel.

I have followed the Sample code for iMX6 SabreSD to use MIPI CSI camera with virtual channel 3.

Still I am getting " mipi csi2 can not receive sensor clk1'

How to solve this issue?

Thanks

Saurabh

ラベル(1)
1 解決策
814件の閲覧回数
saurabh206
Senior Contributor III

I am able to fixed this issue.

It was hardware issue.

Following patch is the only modification required for Virtual channel 3.

Sample code for iMX6 SabreSD to use MIPI CSI camera with virtual channel 3.

Thanks

Saurabh

元の投稿で解決策を見る

2 返答(返信)
815件の閲覧回数
saurabh206
Senior Contributor III

I am able to fixed this issue.

It was hardware issue.

Following patch is the only modification required for Virtual channel 3.

Sample code for iMX6 SabreSD to use MIPI CSI camera with virtual channel 3.

Thanks

Saurabh

814件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Saurabh ,

   Good job !

Weidong

0 件の賞賛
返信