Sample code for iMX6 SabreSD to use MIPI CSI camera with virtual channel 3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sample code for iMX6 SabreSD to use MIPI CSI camera with virtual channel 3

Sample code for iMX6 SabreSD to use MIPI CSI camera with virtual channel 3

It is based on 3.0.35 GA 4.1.0 BSP.

 

0001-Correct-mipi-camera-virtual-channel-setting-in-ipu_c.patch

It is the updated IPU code for MIPI ID and SMFC setting in ipu_capture.c. These setting should not be combined with MIPI virtual channel value, they shoule be fixed with ID 0.

 

0002-Use-virtual-channel-3-for-ov5640-mipi-camera-on-iMX6.patch

The sample code to modify ov5640_mipi camera to use virtual channel 3 on SabreSD board.

 

The followed command can be used to verify the mipi camera function after booted into Linux:

$ gst-launch mfw_v4lsrc capture-mode=1 device=/dev/video1 ! mfw_v4lsink

 

 

2014-09-30 update:

Added the patch for 3.10.17_GA1.0.0 BSP. "L3.10.17_1.0.0_mipi_camera_virtual_channel_3.zip"

 

Attachments
Comments

Hi Qiang_FSL

Do you know which virtual channel number using in OV5640_mipi.c base on 3.14.28 BSP ?

Apollo Chang.

It is vc=1 in default BSP for ov5640_mipi.

Hi Qiang Li

Thanks....

But why our device tree is define (i.MX6Q)

&mipi_csi {

    status = "okay";

    ipu_id = <0>;

    csi_id = <1>;

    v_channel = <0>;

    lanes = <2>;

};

In default BSP, the v_channel from mipi_csi of the device tree is not used as real virtual channel setting, it must be 0.

And the csi_id from ov5640_mipi of the device tree is used as the real virtual channel setting in driver.

They will make user confused, that's why I created these patches to make everything more reasonable.

Hi Qiang_FSL​

Thanks...

It is very help us to know more detail.

Hi, Qiang Li:

     DI include vc and datatype. why the ipu driver ignore vc. like follow:

pastedImage_0.png

VC is not used in IPU side, it must be filled with 0.

I knew that, DI create by camera in the packet. But ipu-csi CSI_DI register is a match value, route the packet where to go?

No, the DI tells the IPU to capture which kind of data, for example YUV422 or RGB888.

No ratings
Version history
Last update:
‎09-09-2014 12:54 AM
Updated by: