MIPI CSI Line Interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIPI CSI Line Interrupt

ソリューションへジャンプ
2,421件の閲覧回数
t-sugiyama
Contributor III

Hello,

I have a question about the LINE_END interrupt of the MIPI CSI of i.MX8Mmini.
I set LINE_INTR of "Line Interrupt Ratio" to 0x1.
In this case, when is the LINE_END interrupt timing of "Interrupt source register 1"?
Is the size of the received data relevant?

Thanks.

Tetsuya.

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
2,264件の閲覧回数
art
NXP Employee
NXP Employee

With this setting, the LINE_END interrupt will be raised each time the Line End packet is detected on a specific MIPI CSI lane.

Best Regards,
Artur

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,265件の閲覧回数
art
NXP Employee
NXP Employee

With this setting, the LINE_END interrupt will be raised each time the Line End packet is detected on a specific MIPI CSI lane.

Best Regards,
Artur

0 件の賞賛
返信