MIPI CSI Line Interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI CSI Line Interrupt

Jump to solution
2,419 Views
t-sugiyama
Contributor III

Hello,

I have a question about the LINE_END interrupt of the MIPI CSI of i.MX8Mmini.
I set LINE_INTR of "Line Interrupt Ratio" to 0x1.
In this case, when is the LINE_END interrupt timing of "Interrupt source register 1"?
Is the size of the received data relevant?

Thanks.

Tetsuya.

Tags (1)
0 Kudos
Reply
1 Solution
2,262 Views
art
NXP Employee
NXP Employee

With this setting, the LINE_END interrupt will be raised each time the Line End packet is detected on a specific MIPI CSI lane.

Best Regards,
Artur

View solution in original post

0 Kudos
Reply
1 Reply
2,263 Views
art
NXP Employee
NXP Employee

With this setting, the LINE_END interrupt will be raised each time the Line End packet is detected on a specific MIPI CSI lane.

Best Regards,
Artur

0 Kudos
Reply