MIMXRT1024 flash resident second bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1024 flash resident second bootloader

2,393件の閲覧回数
PaulH_68
Contributor I

Hi
Please can you give me some guidance as to how to recompile the RT1024 bootloader example in MCUXpresso to run XIP from flash as per AN12604. Can we use Reliable Update?

Thanks

0 件の賞賛
返信
3 返答(返信)

2,386件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @PaulH_68 ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
According to your statement, it seems that you want to port the AN12604 to the RT1024, moreover, the demo is built by the MCUXpresso IDE. Is my understanding right?
If yes, there's no guide or similar documents to illustrate the porting steps until now, in a word, it needs the developer to do it by himself.
Definitely, you can apply for some support from us if you encounter some troubles.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,346件の閲覧回数
PaulH_68
Contributor I

Yes you are correct in what we are trying to do.
Now I have tried the OTA flashloader example for MIMXRT1060-EVK on MIMXRT1062-EVK board using SDK v 2.8.4 and MCUXpresso v11.5.1 but it does not respond to <blhost -p COM4 -j -- get-property 1> command. I tried running from flash boot and in debug mode. I also tried the RAM flashloader example for RT1062 in debug which also does not respond to blhost command.
I loaded "Hello World" example to check hardware and it is ok!
I can run RAM flashloader example for RT1052 which does work ok on MIMXRT1050-EVK.
Any reason why RT1062 OTA flashloader should not work?
When OTA flashloader for RT1062 works, then I can port it for RT1052 and RT1024

Thanks

0 件の賞賛
返信

2,342件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @PaulH_68 ,
Regarding OTA flashloader demo, I'd like to suggest you refer to the post to test.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信