MIMX8MP MIPI-CSI2 Custom Camera Capture in non-continuous clock mode.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMX8MP MIPI-CSI2 Custom Camera Capture in non-continuous clock mode.

3,557 Views
guffigubber
Contributor II

Hi!
After successfully launching the camera with continuous clock in this topic, I continued to connect another camera. 
I can't get frames.

Camera parameters: 2 lanes mipi, pixel clock - 32.5MHz, width - 1280, height - 1024, fps 20. 

I can't understand what I'm doing wrong. Clock waveform attached.

 

camera_0: camera_0_mipi@3e {
	compatible = "camera_0";
	reg = <0x3e>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_csi0_rst>, <&pinctrl_csi0_pwn>;
	csi_id = <0>;
	reset-gpios = <&gpio3 19 GPIO_ACTIVE_LOW>;
	enable-gpios = <&gpio3 20 GPIO_ACTIVE_HIGH>;
	mipi_csi;
	status = "okay";

	port {
		camera_mipi_0_ep: endpoint {
			bus-type = <4>;
			data-lanes = <1 2>;
			clock-lanes = <0>;
                        clock-noncontinuous;
			remote-endpoint = <&mipi_csi0_ep>;
		};
	};
};

&mipi_csi_0 {
	#address-cells = <1>;
	#size-cells = <0>;
	status = "okay";
	port@0 {
		reg = <0>;
		mipi_csi0_ep: endpoint {
			remote-endpoint = <&camera_mipi_0_ep>;
			data-lanes = <2>;
			csis-hs-settle = <13>;
			csis-clk-settle=<2>;
			csis-wclk;
		};
	};
	
};

&mipi_csi_1 {
	#address-cells = <1>;
	#size-cells = <0>;
	status = "disabled";
};

&cameradev {
	status = "okay";
};

&isi_0 {
	status = "okay";

	cap_device {
		status = "okay";
	};

//	m2m_device {
//		status = "okay";
//	};
};

&isi_1 {
	status = "disabled";

	cap_device {
		status = "disabled";
	};
};

&isp_0 {
    status = "disabled";
};

&isp_1 {
	status = "disabled";
};

&dewarp_0 {
    status = "disabled";
};

 

 

Tags (3)
0 Kudos
Reply
3 Replies

3,472 Views
guffigubber
Contributor II

It turns out that the processor does not see the data at all? Why can this be so?

[   41.188511] mxc-mipi-csi2.0: mipi_csis_s_stream: 1, state: 0x0
[   41.188617] mxc-mipi-csi2.0: fmt: 0x2006, 1280 x 1024
[   41.203853] mxc-mipi-csi2.0: --- mipi_csis_s_stream ---
[   41.203860] mxc-mipi-csi2.0:         CSIS_VERSION[0]: 0x03060301
[   41.203863] mxc-mipi-csi2.0:        CSIS_CMN_CTRL[4]: 0x00004905
[   41.203867] mxc-mipi-csi2.0:        CSIS_CLK_CTRL[8]: 0x000f0000
[   41.203870] mxc-mipi-csi2.0:          CSIS_INTMSK[10]: 0x0fffff1f
[   41.203874] mxc-mipi-csi2.0:          CSIS_INTSRC[14]: 0x00000000
[   41.203878] mxc-mipi-csi2.0:      CSIS_DPHYSTATUS[20]: 0x000000f1
[   41.203881] mxc-mipi-csi2.0:        CSIS_DPHYCTRL[24]: 0x00000007
[   41.203885] mxc-mipi-csi2.0:     CSIS_DPHYBCTRL_L[30]: 0x000001f4
[   41.203888] mxc-mipi-csi2.0:     CSIS_DPHYBCTRL_H[34]: 0x00000000
[   41.203892] mxc-mipi-csi2.0:     CSIS_DPHYSCTRL_L[38]: 0x00000000
[   41.203895] mxc-mipi-csi2.0:     CSIS_DPHYSCTRL_H[3c]: 0x00000000
[   41.203899] mxc-mipi-csi2.0:   CSIS_ISPCONFIG_CH0[40]: 0x00001078
[   41.203902] mxc-mipi-csi2.0:   CSIS_ISPCONFIG_CH1[50]: 0x000008fd
[   41.203906] mxc-mipi-csi2.0:   CSIS_ISPCONFIG_CH2[60]: 0x000008fe
[   41.203910] mxc-mipi-csi2.0:   CSIS_ISPCONFIG_CH3[70]: 0x000008ff
[   41.203913] mxc-mipi-csi2.0:    CSIS_ISPRESOL_CH0[44]: 0x04000500
[   41.203917] mxc-mipi-csi2.0:    CSIS_ISPRESOL_CH1[54]: 0x80008000
[   41.203920] mxc-mipi-csi2.0:    CSIS_ISPRESOL_CH2[64]: 0x80008000
[   41.203924] mxc-mipi-csi2.0:    CSIS_ISPRESOL_CH3[74]: 0x80008000
[   41.203927] mxc-mipi-csi2.0:     CSIS_ISPSYNC_CH0[48]: 0x00000000
[   41.203931] mxc-mipi-csi2.0:     CSIS_ISPSYNC_CH1[58]: 0x00000000
[   41.203934] mxc-mipi-csi2.0:     CSIS_ISPSYNC_CH2[68]: 0x00000000
[   41.203938] mxc-mipi-csi2.0:     CSIS_ISPSYNC_CH3[78]: 0x00000000
[   41.203941] mxc-mipi-csi2.0: --- mipi_csis_s_stream ---
[   41.203945] mxc-mipi-csi2.0:    GPR_GASKET_0_CTRL[60]: 0xffff8000
[   41.203948] mxc-mipi-csi2.0:   GPR_GASKET_0_HSIZE[64]: 0xffff8000
[   41.203952] mxc-mipi-csi2.0:   GPR_GASKET_0_VSIZE[68]: 0xffff8000
[   42.466803] mxc-mipi-csi2.0: status: 02000000
.....
[   43.758314] mxc-mipi-csi2.0: status: 00200000
[   43.762729] mxc-mipi-csi2.0: status: 02000000
[   43.808155] mxc-mipi-csi2.0: status: 00200000
[   43.812575] mxc-mipi-csi2.0: status: 02000000
[   43.858001] mxc-mipi-csi2.0: status: 00200000
[   43.862418] mxc-mipi-csi2.0: status: 02000000
[   43.895955] mxc-mipi-csi2.0: mipi_csis_s_stream: 0, state: 0x0
[   43.895968] mxc-mipi-csi2.0: Frame End events: 0
[   43.902123] mxc-mipi-csi2.0: Frame Start events: 0
[   43.909775] mxc-mipi-csi2.0: Non-image data after odd frame events: 0
[   43.919073] mxc-mipi-csi2.0: Non-image data before odd frame events: 0
[   43.928458] mxc-mipi-csi2.0: Non-image data after even frame events: 0
[   43.935673] mxc-mipi-csi2.0: Non-image data before even frame events: 0
[   43.942283] mxc-mipi-csi2.0: Unknown Error events: 0
[   43.947244] mxc-mipi-csi2.0: CRC Error events: 0
[   43.951857] mxc-mipi-csi2.0: ECC Error events: 0
[   43.956470] mxc-mipi-csi2.0: FIFO Overflow Error events: 0
[   43.961951] mxc-mipi-csi2.0: Lost Frame End Error events: 0
[   43.967519] mxc-mipi-csi2.0: Lost Frame Start Error events: 0
[   43.973261] mxc-mipi-csi2.0: SOT Error events: 0

 

0 Kudos
Reply

3,520 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

Are you using the MX8Mplus EVK? you have a device tree in linux BSP that support two cameras MIPI-CSI.

Regards

0 Kudos
Reply

3,490 Views
guffigubber
Contributor II

Hello,

I'm using cpu your partner Forlinx FETMX8MP-C. with a kernel version 5.4.70.

I haven't problem problem running two cameras at the same time (4 lanes, continuous clock mode, 1920x1080@30, 148.5MHz pixel clock). 

I have a problem connecting a specific camera (2 lanes mipi, pixel clock - 32.5MHz, 1280х1024@20). It issues a clock only at the moment of frame transfer. Clock waveform attached in topic start.

Thank You!

0 Kudos
Reply