IMX8MP ISI.0 MIPI-CSI2 Camera Capture

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MP ISI.0 MIPI-CSI2 Camera Capture

ソリューションへジャンプ
3,970件の閲覧回数
guffigubber
Contributor II

Hi!

I have a processor IMX8MP with a kernel version 5.4.70.

I am trying to connect a camera to csi0 (camera --> mipi csi 0 --> isi0 --> /dev/video0).

On another input (camera --> mipi csi 1 --> isi0 --> /dev/video1) it works without problems with the same settings.

What could be the problem?

 

camera_0: camera_0_mipi@3e {
	compatible = "camera_0";
	reg = <0x3e>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_csi0_rst>, <&pinctrl_csi0_pwn>;
	csi_id = <0>;
	reset-gpios = <&gpio3 19 GPIO_ACTIVE_LOW>;
	enable-gpios = <&gpio3 20 GPIO_ACTIVE_HIGH>;
	mipi_csi;
	status = "okay";

	port {
		camera_mipi_0_ep: endpoint {
			bus-type = <4>;
			data-lanes = <1 2 3 4>;
			clock-lanes = <0>;
			remote-endpoint = <&mipi_csi0_ep>;
		};
	};
};

camera_1: camera_1_mipi@3c {
	compatible = "camera_1";
	reg = <0x3c>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_csi1_rst>, <&pinctrl_csi1_pwn>;
	csi_id = <1>;
	reset-gpios = <&gpio1 6 GPIO_ACTIVE_LOW>;
	enable-gpios = <&gpio2 11 GPIO_ACTIVE_HIGH>;
	mipi_csi;
	status = "okay";
	port {
	        camera_mipi_1_ep: endpoint {
		        bus-type = <4>;
			data-lanes = <1 2 3 4>;
			clock-lanes = <0>;
			remote-endpoint = <&mipi_csi1_ep>;
		};
	};
};


&mipi_csi_0 {
	#address-cells = <1>;
	#size-cells = <0>;
	status = "okay";
	port@0 {
		reg = <0>;
		mipi_csi0_ep: endpoint {
			remote-endpoint = <&camera_mipi_0_ep>;
			data-lanes = <4>;
			csis-hs-settle = <13>;
			csis-clk-settle=<2>;
			csis-wclk;
		};
	};
	
};

&mipi_csi_1 {
	#address-cells = <1>;
	#size-cells = <0>;
	status = "okay";

	port@1 {
		reg = <1>;
		mipi_csi1_ep: endpoint {
			remote-endpoint = <&camera_mipi_1_ep>;
			data-lanes = <4>;
			csis-hs-settle = <13>;
			csis-clk-settle=<2>;
			csis-wclk;
		};
	};
};

&cameradev {
	status = "okay";
};

&isi_0 {
	status = "okay";

	cap_device {
		status = "okay";
	};

//	m2m_device {
//		status = "okay";
//	};
};

&isi_1 {
	status = "okay";

	cap_device {
		status = "okay";
	};
};

&isp_0 {
    status = "disabled";
};

&isp_1 {
	status = "disabled";
};

&dewarp_0 {
    status = "disabled";
};
タグ(3)
0 件の賞賛
返信
1 解決策
3,933件の閲覧回数
guffigubber
Contributor II

Thank you! Problem solved!

The camera started sending video when turned on. And CSI1 could immediately capture the video.
For CSI0, you need to turn off the camera so that it does not send video.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,945件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

The camera works on continous mode, it can't work DSI+CSI0, after change to non-continous mode, it can work DSI+CSI0.

 

Regards

0 件の賞賛
返信
3,934件の閲覧回数
guffigubber
Contributor II

Thank you! Problem solved!

The camera started sending video when turned on. And CSI1 could immediately capture the video.
For CSI0, you need to turn off the camera so that it does not send video.

0 件の賞賛
返信