MIMX8ML8DVNLZAB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,826件の閲覧回数
JyotiVaishnav
Contributor II

Hello NXP team, 
We are designing a hardware platform using
MIMX8ML8DVNLZAB processor. 

We required a qualified LPDDR and eMMC list of MIMX8ML8DVNLZAB.

Please help us to get the details asap.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,808件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @JyotiVaishnav ,

I hope you are doing well.

Regarding eMMC, i.MX8MP processor supports MMC standard, up to version 5.1. It supports 1-bit/4-bit/8-bit MMC mode. Any eMMC meeting this requirement can be used with i.MX8MP processor.

Regarding DRAM, one can refer to the below link which mentions the list of validated memories.
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Quad-8M-Mini-8M-Nano-8M-Plus-max...

One can also refer to the i.MX8MP EVK's schematic to take the reference of qualified part numbers of eMMC and DRAM.

i.MX 8M Plus LPDDR4 EVK Compute Module Design Files 

Thanks & Regards,
Ritesh M Patel

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,809件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @JyotiVaishnav ,

I hope you are doing well.

Regarding eMMC, i.MX8MP processor supports MMC standard, up to version 5.1. It supports 1-bit/4-bit/8-bit MMC mode. Any eMMC meeting this requirement can be used with i.MX8MP processor.

Regarding DRAM, one can refer to the below link which mentions the list of validated memories.
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Quad-8M-Mini-8M-Nano-8M-Plus-max...

One can also refer to the i.MX8MP EVK's schematic to take the reference of qualified part numbers of eMMC and DRAM.

i.MX 8M Plus LPDDR4 EVK Compute Module Design Files 

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信