MIMX8ML8DVNLZAB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMX8ML8DVNLZAB

Jump to solution
1,827 Views
JyotiVaishnav
Contributor II

Hello NXP team, 
We are designing a hardware platform using
MIMX8ML8DVNLZAB processor. 

We required a qualified LPDDR and eMMC list of MIMX8ML8DVNLZAB.

Please help us to get the details asap.

0 Kudos
Reply
1 Solution
1,809 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @JyotiVaishnav ,

I hope you are doing well.

Regarding eMMC, i.MX8MP processor supports MMC standard, up to version 5.1. It supports 1-bit/4-bit/8-bit MMC mode. Any eMMC meeting this requirement can be used with i.MX8MP processor.

Regarding DRAM, one can refer to the below link which mentions the list of validated memories.
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Quad-8M-Mini-8M-Nano-8M-Plus-max...

One can also refer to the i.MX8MP EVK's schematic to take the reference of qualified part numbers of eMMC and DRAM.

i.MX 8M Plus LPDDR4 EVK Compute Module Design Files 

Thanks & Regards,
Ritesh M Patel

View solution in original post

0 Kudos
Reply
1 Reply
1,810 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @JyotiVaishnav ,

I hope you are doing well.

Regarding eMMC, i.MX8MP processor supports MMC standard, up to version 5.1. It supports 1-bit/4-bit/8-bit MMC mode. Any eMMC meeting this requirement can be used with i.MX8MP processor.

Regarding DRAM, one can refer to the below link which mentions the list of validated memories.
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Quad-8M-Mini-8M-Nano-8M-Plus-max...

One can also refer to the i.MX8MP EVK's schematic to take the reference of qualified part numbers of eMMC and DRAM.

i.MX 8M Plus LPDDR4 EVK Compute Module Design Files 

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply